Tool/software:
Hi TI
I'm designing a board using LM73606, and the concept is as follows.
Inpput V : 12V
Output V : 3.3V or 3.8V
Fsw : 500Khz
SYNC/MODE : auto mode
Question)
1. Is there no problem with the input, output cap quantity and value?
2. I'm trying to use a power inductor 4.7uH that's available for both 3.3V or 3.8V, is there any problem?
And can you recommend any specifications or part numbers?
3. What should I do with Sync mode pins NC or GND?
4. What is bias cap not mount or mount?
5. What is the result of the full circuit review? Any points to modify?
Br
chulho.Jang