This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC14: Vol value shooting above vaues given in DS, need help.

Part Number: SN74HC14
Other Parts Discussed in Thread: LM2670, SN74AHC14, SN74HCS14, SN74LV14A

Tool/software:

Hello Team

I am using SN74HC14DR to give inputs coming into my board to a microcontroller. The Vcc is given through a regulated 5V power supply (LM2670).

As per datasheet I should be getting a VOL of max 0.33V but we are observing it comes to 0.730V in our case. As I mentioned the Vcc is 5V and the input to the individual schmitt trigger channels are around 4.5V.

Why could this be happening. Is there anything we need to consider? As an additional info : we are not observing this issue while using MC74HC14ADR2G in same application.

Thank You