This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108:About the 200kΩ Bias Resistor Value

Part Number: LSF0108

Tool/software:

I am planning to use the LSF0108 for bidirectional voltage level shifting.

It will be used with Vref_A = 1.8V and Vref_B = 3.3V, but I would like to know if the 200kohm bias resistor between VCCB and Vref_B can be replaced with a 180kohm or 220kohm resistor.

Could you please explain why it is necessary to use a fixed value of 200kohm?