Other Parts Discussed in Thread: SN74AHCT32
Tool/software:
I have currently built a circuit using SN74AHCT32 Logic gate. I need to connect the VCC power supply, but I don't know how much current it will consume,
so I need to make a judgment.I have currently built a circuit using SN74AHCT32 Logic gate.
I need to connect the VCC power supply, but I don't know how much current it will consume, so I need to make a judgment.
When everything output changes to 1, how much can we expect to consume?
Currently, the output of each channel is connected to the input of the next channel. (ex 1ch output -> 2ch input)
The output of the last channel is connected to another logic gate input.The output of the last channel is connected to another logic gate input.
I understand that the input impedance of logic gates is very high, so can I assume that the current consumed from VCC is also small? Can I assume it is in the nA range?