Other Parts Discussed in Thread: SN74HCT240, UCC23513
Tool/software:
Hi TEAM,
My customer want to upgrade the temperature range for their machine and the do some change from SN74HCT240 to SN74AHCT240.
But they found some output oscillation issue on output pin. I found there are some differences on output spec between these two devices. but I don't know which one is the biggest influencer this issue. Could you kindly tell me which differences on output structure will cause this ? and how to deal with the overstress on output?
Schematic

B-SN74AHCT240(125℃)ch2 input,ch4 output. positive voltage spike is 5.980V, over max VCC(5V)+0.5V. The device is from SHE FAB.


C-SN74HCT240(85℃)ch1 is output, no obvious overstress. From RFAB


BR
Emma