Part Number: SN74LVC1G125
Tool/software:
Hello TI team,
We use SN74LVC1G125, and the full part number is SN74LVC1G125DRYR
In the SPEC, there are two definitions for the DRY PACKAGE OUTLINE
Which one should I choose for this part number?

Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G125
Tool/software:
Hello TI team,
We use SN74LVC1G125, and the full part number is SN74LVC1G125DRYR
In the SPEC, there are two definitions for the DRY PACKAGE OUTLINE
Which one should I choose for this part number?

Thanks
Hello Clemens,
Thank you for your reply. For the control of the part, there should only be a single dimension specification. However, these two drawings have different dimension specifications, not just differences in assembly sites. (The body heights of the two are also different)
Could you clearly confirm whether this complies with DRY006A or DRY006B? (SN74LVC1G125DRYR)
The pads and the footprints have exactly the same size in both variants, except for pin 1, which is longer in variant A. So you probably want to use DRY0006A for your board.
Hello Clemens,

Thank you for your reply.
The height definitions of the two are also different. Which one should I choose?
Could you clearly confirm whether this complies with DRY006A or DRY006B? (SN74LVC1G125DRYR)
Thanks
There is no specified minimum. So over all possible devices, you only know that the maximum is 0.6 mm.