Tool/software:
Hi team,
What is the maximum allowable load capacity of this device?
I would also like to know the propagation delay at that time.
Best Regards,
Ryu.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
What is the maximum allowable load capacity of this device?
I would also like to know the propagation delay at that time.
Best Regards,
Ryu.
This device is not designed to drive large capacitive loads.
Loads up to about 70 pF can be connected directly. For larger capacitances, add a current-limiting series resitor to ensure that you stay below the absolute maximum rating of 50 mA.
For how the load affects the rise/fall time, see [FAQ] What is the output transition rate for a logic device?
Hello Ryu,
I agree with Clemens here. The only thing I would add is all the datasheet timing parameters are captured using a 15pF load capacitor. Any capacitor that's not 15pF will have some impact on these parameters.
Regards,
Josh