Part Number: TXU0104-Q1
Tool/software:
Hi,
I plan to use P/N TXU0104QPWRQ1, and I have a question regarding the configuration:
The device should translate low-speed Single-Ended signals from 1.2 [V] (left) to 5 [V] (right).
In this case VCCA is connected to a 1.2 [V] power-rail, and VCCB is connected to a 5 [V] power-rail.

My question is – Can I connect the output-enable (OE) pin to 3.3 [V] voltage level signal, or it can cause stress (in time) and harm the device?
(since VCCA = 1.2 [V])
According to the datasheet, the OE can be pulled either to VCCA or VCCB.
Is a voltage in the middle will be acceptable?

Best regards,
Avihay.