This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T245: Vol issue

Part Number: SN74AVC4T245

Tool/software:

Hi experts,

Customer used SN74AVC4T245 and have an issue that the Vol is not low enough at 3.3V side in below system block.

Wondering is there any internal pullups in the chip? or do you have any idea what might goes wrong? 

   

Regards,

Allan

  • The SN74AVC4T245 does not have internal pull-up resistors. Its output will pull the line up only when its input is high.

    When the VOL is too high, then some other device or resistor is pulling the line high. Try disconnecting them to see which one is responsible.

  • Hello Allan,

    What is the VOL value the customer is seeing? Like Clemens mentioned, if VOL is above the datasheet spec then something is pulling the line high. I would remove anything connected to the level shifter output and measure at the pin.

    Regards,

    Josh