This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC374: Logic forum

Part Number: SN74HC374

Tool/software:

We found TI part CFN320107-R (MPN:  SN74HC374DWR ), with two body mark on top Lane, " 48CX0CK" and " 48CX1CK"  but we found about 30% defect rate for this part and All Failed parts with Mark" 48CX1CK", what's the difference between "1" and "0"?? 

But I got feedback from TI China Engineer below: 

 Martin

48CX0CK" and " 48CX1CK are different lot
Please discuss so high 30% failure with application team or on E2E.ti.com.
1)Board mark 48CX0CK is pass. The actual waveform is displayed in ICT debug mode. For details, see the following screenshot
      
 
 2)Board mark 48CX1CK is fail. The actual waveform is displayed in ICT debug mode. For details, see the following screenshot.
    
  
Bellow is schedule for this part: