This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3825: I need to design a parallel Buck with interleaved signals.

Part Number: UC3825
Other Parts Discussed in Thread: UCC28220, LM5032

Tool/software:

I need to design a parallel Buck with interleaved signals.

Can you suggest me what PWM control IC to use?
I need the PWM signal to be output as shown below Vgs1  and Vgs2.
Buck
Vin=300V Vo = 250V

Duty : 83%
Fs : 85kHz