Other Parts Discussed in Thread: TXU0304,
Tool/software:
We are using LSF0204RUTR for our design we are able to communicate to CAN IC upto 5MHz via SPI if i go higher than 5Mhz(to10Mhz), i am not getting any response from the CAN IC.
When we probed the SPI lines the 5V side is reaching up to 2.4V only.
the max current sink capability of my processor is 16mA so i can't reduce the pull up values very low, current value is 2.2Kohm.
Could anyone help us to proceed further?