SN74AVC4T774-Q1: Electrical comparison to NEXPERIA 74AVC4T774-Q100

Part Number: SN74AVC4T774-Q1
Other Parts Discussed in Thread: SN74AXC4T774-Q1

Tool/software:

Hi,

My customer is comparing SN74AVC4T774-Q1 to NEXPERIA 74AVC4T774-Q100.
There are some differences in the electrical parameters and they have questions about this.

They also look at SN74AXC4T774-Q1 since it seems to be closer to the NEXPERIA device, but differs in part number.

Screenshot from SN74AVC4T774-Q1:

Screenshot from NEXPERIA 74AVC4T774-Q100. They expected this in the TI datasheet as well:

While the values are identical up to supply voltage of 1.95V, they differ greatly in are >1.95V to 3.6V.
Also, the max allowed LOW input levels in the TI device are larger than the allowed HIGH input levels. How can this be?

Screenshot from SN74AXC4T774-Q1. They would have expected this in SN74AVC4T774-Q1 datasheet:

Best regards