This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS74: Spice model does not seem to work in PSpice for TI

Part Number: SN74HCS74


Tool/software:

Hi,

I have imported the SN74HCS74 cir file correctly in PSpice and simulation is now reporting 3x that NO1 pin is not connected. All pins have been connected. Could it be possible that this model is not compatible with pspice?

Regards,

Klaas-Jan

  • To be more specific.

    the schema is:

    the error is:

    --------------- INFO(ORPROBE-3209): Simulation Profile: SCHEMATIC1-sim ---------------
    INFO(ORPROBE-3183): Simulation running...
    ** Profile: "SCHEMATIC1-sim" [ D:\work\circuits\autorangecurrentmeasure\topcurrentRev2logsigmaaddon\pspiceforti\pulseandflipfloptes
    Reading and checking circuit
    ERROR(ORPSIM-15141): Less than 2 connections at node X_U11.XU6.XU1.XU1.NO1.
    ERROR(ORPSIM-15141): Less than 2 connections at node X_U11.XU5.XU1.XU1.NO1.
    ERROR(ORPSIM-15141): Less than 2 connections at node X_U11.XU10.XU1.XU1.NO1.
    ERROR(ORPSIM-15141): Less than 2 connections at node X_U11.XU9.XU1.XU1.NO1.
    ERROR(ORPSIM-15141): Less than 2 connections at node X_U11.XU8.XU1.XU1.NO1.
    ERROR(ORPSIM-15141): Less than 2 connections at node X_U11.XU1.XU1.XU1.NO1.
    Circuit has errors ... run aborted
    See output file for details
    INFO(ORPROBE-3188): Simulation aborted

  • Hi Klaas,

    Let me send this to our modeling expert in the team to figure out the issue.

  • I also want to add that this model is also not working in LT spice while the SN74LVC74 model is working. Looks like there is a something wrong with the spice model. Any news?

  • Here Klaas, try this version.

    1033.SN74HCS74.CIR