Part Number: TXB0108
Tool/software:
Hi,
My customer is using this device to translate from 1.8V to 3.3V
What is the minimum pull up resistance required to guarantee correct direction? (for both directions?) Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0108
Tool/software:
Hi,
My customer is using this device to translate from 1.8V to 3.3V
What is the minimum pull up resistance required to guarantee correct direction? (for both directions?) Thank you!
The TXB does not have a direction. The input and output buffers on both sides are always active, and the drive strength is extremely low (20 µA) to allow other devices to override the voltage. Therefore, any pull-up resistors must be larger than 50 kΩ (see section 7.3.5 of the datasheet).
If you have a pull-up, then it is likely that you also need one on the other side.