This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC126A: Output Behaviour When Not Supplied

Part Number: SN74LVC126A


Tool/software:

Hi,

what is the expected behaviour of the SN74LVC126A outputs in case the supply voltage (VCC) and output enable (OE) are not supplied / low / equal to GND? Thanks in advance.

Best regards,

Jakob

  • The output will be disabled, but the body diode of the output's P-channel MOSFET creates a current path from the output to the VCC pin.

  • So if VCC is low (GND) and a 200k resistor is connected from the output to 1V8 the body diode should not be conducting right?

    I am asking because this is the exact setup I am facing: VCC and OE low / GND and a 200k resistor connected from the buffer output to 1V8. I am measuring about 0,4 V at the output in that case. But if the body diode is not conducting, then how is the signal pulled down?

  • My bad. The P-FET source is connected to the VCC pin (which is GND in my case) and drain is connected to the output. Thus, the body diode of the P-FET is in fact conducting which is why the output if not "high" (0,4 V) in my case. Thanks for the help.