This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using Darlington Pair

Other Parts Discussed in Thread: ULN2003A

Dear All,

I am using a controller with I/O levels at 3.3V and as i need to drive some motors i am using ULN2003A from TI .

We are having two voltage domains in the PCB

 a. 3.3V/5A ( for processor and ethernet ) and

 b. 5V/5A for all motors and peripherals.

The motor operates at 5V , please suggest how to manage should we use a level translator to connect the controller to ULN2003A

 

Thank you in advance,

 

Best Regards,

San

  • Hi,

    with the ULN2003A you just need a high level of 3V to get a collector current of 300 mA (datasheet page 5). So, why not connect the output pin of the controller directly? The output pin has to drive less than 1 mA (datasheet page 11) which it can drive easily.

    Best regards,
    Edwin Krasser