This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXV0108-Q1: TXV0108-Q1

Part Number: TXV0108-Q1


Tool/software:

Hi,

I would like to verify if I placed 3.3V for VCCB and for VCCA 1.8V, the signals A1 to A8 are driven by 3.3V

Is the component will work correctly or damaged?

Note:

I saw in the datasheet section 7.3.4 and it is not clear to me

7.3.4 Over-Voltage Tolerant Inputs Input signals to this device can be driven above the supply voltage so long as they remain below the maximum input voltage value specified in the Recommended Operating Conditions.