This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LXC1T14: Design Questions

Part Number: SN74LXC1T14


Tool/software:

Dear *,

we would like to use SN74LXC1T14 for level translation from 1.8V to 3.3V.

The 1.8V is generated from 3.3V via LDO ( TLV77433PDQN, t_start_typ = 400us).

The input requires a pull-up, in datasheet says that the pull-p should be no larger than 15k , so we can use 10k?

The output will be connected to reset IC ( TLV809EA29DPW)  to the MR pin that has internal pull-up of 100k.

Do you see any problem wit this configuration?

Best Regards,

d.