Part Number: SN74LS156
Other Parts Discussed in Thread: SN74AHC238, TPL7407LA, TMUX4052
Tool/software:
Hi all
I'm looking for an alternative for the SN74LS156 decoder/demultiplexer IC which would have the following characteristics:
- 3-to-8 decoder with "select-low" outputs,
- operating with supply voltages down to 3 V,
- open-collector (or open-drain) outputs,
- allowed off-state voltage of 15 V on outputs.
Does this kind of logic IC even exist? Could I use CD4028 + 8 discrete transistors to achieve these requirements? Although I am not sure if the CD4028 could operate with 3 V supply.
Thank you!