Other Parts Discussed in Thread: SN74AHC245-EP, SN74AHC244-EP, SN74LVC8T245-EP, SN74LVCH16T245-EP
Tool/software:
Here's my design problem. I have 13 inputs that need to support 5V TTL logic levels (ViL: 0 - 0.8V, ViH: 2V - 5V) and then level shift down to 3.3V. I'm working on a SiP design so package size is critical.
The SN74LVTH16245A-EP is ideal from a spec standpoint but the mil-spec package is 16mm x 10mm. That part comes in a VBGA package which would work but that package is only temp rated for -40 - 85C.
1. So I'm looking for 2 things - does anyone know why the temp ratings differ per package?
2. Does anyone have any alternative solution ideas that are smaller than 16mm x 10mm?