Other Parts Discussed in Thread: DAC7562, MSP430F5529, TXB0104
Hi, I am considering the TXB0104 as a level shifter between my MSP430F5529(at 3.3V) and my DAC7562(at 5V). This is a low power, battery operated application.
On the TXB0104, port A will always be an input(from the uC), and port B will alwya be an output(to the DAC).
The data sheet states that my uC will need to be capable of driving + - 2mA minimum, on each output signal, to get correct operation. The data sheet for the uC indicates that it can do this.
This is my question: Is this a continuous 2ma load on each output pin of the uC ? Or is this current only needed when changing directions ?
I would prefer that my uC not need to source or sink more than 50uA continuously, on each output pin.
Thank you for the help.
Roy Nordstrom