Other Parts Discussed in Thread: CSD16327Q3, SN74LVC00A, UCC44273, SN74LVC2G34, SN74LVC125A
Tool/software:
Hi,
I want to drive 1 mosfet with 1 flip flop, and 2 other mosfets + 1 NAND with other flip flop with this ic:
output currents:
SN74HCS74 DFF: absolute max 35ma, no high/low level output current specified.
A)
one Q output is driving a CSD16301Q2A and a CSD16327Q3
and 1 input pin of a SN74LVC00A NAND
B)
the Q output of the other is driving just a CSD16301Q2A
I see that the max input capacitances of the mosfets are respectively:
CSD16301Q2A 340
CSD16327Q3 1300pf
The latter one is absolutely crucial to my design.
I am simulating this with spice models.
I first was driving these mosfets through a 5ohm resistor. They seem to max out at +-70ma in the simulation.
When i change it to 50 ohm, it is around +-20x20ma=40ma in case (A), and 32ma in case.
These are very short pulses though (it spends 8 nano seconds above 24ma in case B).
Is it a problem to drive the mosfets in case A and B with the logic gates above with 5 ohm resistors and 70ma simulated going from the logic to the gate.
And in general: is it a problem that there are short pulses above the maximum rating?
I really have trouble finding clear information on this.
I have also tested with a SNx4LVC74A DFF. This has a max output current rating of 24ma. Why does the HSC does not have this and to what, if needed, i should limit the current for the HSC DFF.
Also: can i directly connect the above mentioned NANDS/DFF's with without current limiting resistors?
regards,
Klaas-Jan