This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ACT17: Voltage Level Translation with Buffer

Part Number: SN74ACT17

Tool/software:

Hello TI E2E,

I would like to know if SN74ACT17PWRQ1 can be used as a voltage level translator.

The Vih and Vil allows the inputs to be driven from 3.3V, when the VCC is 5V. Hence a simple VLT.

Are there concerns with input protection diodes, or any internal architecture which may affect the input signal level integrity at the input?

I am looking to use this part due to it high drive strength output capabilities in a mixed voltage system.

Thanks,

David