Part Number: SN74LVC07A
Other Parts Discussed in Thread: TPL7407LA
Tool/software:
Hello team,
For the output current of this logic, it's in peak value or DC value?
If it's a DC value, what about the peak value? thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC07A
Other Parts Discussed in Thread: TPL7407LA
Tool/software:
Hello team,
For the output current of this logic, it's in peak value or DC value?
If it's a DC value, what about the peak value? thanks.

Thanks. Here is the test with motor drive control system.
you can see the max. current is up to 54.33mA that is over 50mA SPEC. However, there is no any customer return for this device since this project released to market 3 years ago. Customer would like to make sure if there's no problem with this test waveform. thanks.

This Application is for LED driving like below circuitry. VPU=3.3V, and IC's VCC=3.3V

Regards
Brian
The 50 mA limit is for the worst case and accounts for temperature extremes and manufacturing variations.
But operating at or beyond the limit is likely to degrade the device, and there is no guarantee. Consider using two outputs in parallel (but note the GND pin current limit), or a stronger driver like the TPL7407LA.
Hello Clemens,
Thanks. 50mA is a continue current on spec. however are you able to offer peak current spec with duration time that TI is able to guarantee? Thanks.
Regards
Brian