This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS240-Q1: CAVC8T245QRHLRQ1, SN74HCS240QWRKSRQ1, TPS386596L33DG, TPS386000RGPR

Part Number: SN74HCS240-Q1


Tool/software:

I am reaching out to request Coefficient of Thermal Expansion (CTE) data for a few components. Could you please provide us with the CTE values for the aforementioned part numbers? We would appreciate it if you could provide the CTE values in ppm/°C or ppm/°F, as well as the temperature range over which the values are applicable.

  • Hi Tamren,

    For the HCS device, without an NDA all we can really provide are general ppm values for the various components of the device:

    Copper (primary metal for lead-frame construction) ~17 ppm/⁰C

    NiPdAu coating (outer layer of leadframe) ~13 ppm/⁰C

    Sn coating (alternate outer layer of leadframe) ~21.5 ppm/⁰C

    Mold compound (plastic body) ~12 ppm/⁰C

    Silicon ~2.6 ppm/⁰C

    Best,

    Malcolm