Tool/software:
Hi,
I hope this thread finds you well! In the IR mode we are unable to detect led open detection. We have some below observations.
1) In case of IR mode If the strobe frequency is above 1.4Khz, it is not able to detect the led open in led drive mode priority with voltage mode disable.
2) Below 1.4khz if we remove one of the led and check the 15 flag it is able to detect the led open.
We are giving strobes from the Arduino Uno board with on time-> 100uS, off time-> 100uS.
Regards