Other Parts Discussed in Thread: CD74ACT151
The part that we have experienced some failures with is the Texas Instruments CD74ACT151ME4. I believe that the failures are due to exposure to a condition that violates the specification, however, circuit boards that have been built with an alternate source and have been exposed to the same condition have not experienced the failures.
The alternate source is Fairchild 74ACT151SC.
The condition that I believe is causing the failure is the board has lost power (No VCC), but the input signal is still present (5 VDC).
The specification sheet for the TI part states that Vih maximum is Vcc, so we are violating the specification for the condition where Vcc = 0V, but Vin = 5V.
The specification sheet for Fairchild states that Vih max is Vcc + 0.5V, so we are also violating that specification for the given condition.
The results appear to be different between the manufacturers. No Fairchild parts have failed when exposed to this condition, but the Texas Instruments parts have failed almost every time when exposed to this condition. The part overheats when power is restored, then fails. The component cracks in some instances.
I understand that the component is being exposed beyond the specification limits and we are experiencing latch-up. We are also taking steps to protect against this condition (inserting series resistors on the inputs to keep the input current very low).
My question/concern is, why the Texas Instrument part is so much more sensitive than the Fairchild part, and is this possibly a case of the component being a counterfeit part?