Tool/software:
I am designing a Boost converter using the LM5022.
While selecting the Rsns resistor, I referred to the equation provided in the datasheet.
However, I am having difficulty understanding how this formula is derived.
For reference, here are the specifications of my Boost converter:
- Input Voltage (Vin): 12 V
- Output Voltage (Vout): 18 V
- Output Current (Iout): 3 A
- Switching Frequency (fsw): 200 kHz
- Inductor Value (L): 30 uH
- Output Diode Forward Voltage Drop: 1 V
- Rs1 : 40 ohm
- Csns : 1 nF