Other Parts Discussed in Thread: SN74LVC541A
Tool/software:
Hi,
I want to use the SN74AXC8T245 as a buffer, here is the situation
1. the signals will first pass through an ISO67/ ISO77 digital isolator , 25MHz signals max
2. After the isolators there will be long traces that connect to a lot of chips in parallel so i am thinking of using the SN74AXC8T245 as a buffer after the isolator and before i connect to the chips
( I had some problems before with fewer chips then it comes to the rise time , in design my driver output was 16mA max like the isolator chips so this makes me heavily consider using a buffer since now there are even more chips)
3. All signals are 3v3 and some are default high and some default low
Do you think the SN74AXC8T245 would be a good fit for this application?
I was also considering adding some pull up pull down resistors AFTER the SN74AXC8T245 so that when i put the SN74AXC8T245 in HiZ mode there is a known logic lvl.
This seems ok to me but i want a second opinion, also i am not sure of the pull up value should i go for 10k or 100k? In terms of current there should be no steady state problems BUT i
Am afraid regarding the rise fall times, there is no SPICE model so i cant simulate these transitions. Is there a simplified model that i can use, like a perfect switch with some parasitics ?
Best regards,
Robert