Other Parts Discussed in Thread: THS3491, TLV1871
Tool/software:
Hi,
We are developing a ground based receiver with different inputs and the outputs. Can you suggest the protection circuit/IC which is support for the over voltage protection at the input side and short circuit at the output side.
Input Signal: 1PPS signal
Output Signal: 1PPS signal, IRIG B output each output should be driving capability with 50E impedance.
Suggest the Over voltage protection at input side and Short circuit protection in the output side without degrading the main signal.
And somewhere in the system i want to divide the 1PPS signal into 2 for two different systems, can i use SN74AUP2G17 by providing the same 1PPS signal to the input of channel 1 and 2 then getting 2 output from the buffer. or suggest the best scheme to divide the 1PPS signal.