Part Number: TXS0108E
Other Parts Discussed in Thread: TXU0304, SN74CBTLV3126, SN74CBTLV3245A, TCA39306
Tool/software:
Hi team,
Would like to ask if the TXS0108ENMER is suitable for SPI / eSPI / I2C communication?
Do TI have any other recommended materials for SPI/eSPI/I2C level shift? SPI and eSPI can reach up to 66M, and I2C can reach up to 1M
Current Applications
SPI application is 16Mbps, 1.8V <-> 3.3V;
eSPI application is 20Mbps, 1.8V <-> 1.8V;
400k for I2C applications, 1.8V <-> 3.3V;
The datasheet mentions that it is bi-directional.

From the datasheet, it should be able to support the current design, but there is a problem. The clock data of SPI and eSPI will be delayed, causing reading problems.
I2C seems to have an error in data bidirectional communication

Thanks!
Best regards,
Alice Fan