Other Parts Discussed in Thread: LSF0002,
Tool/software:
① After measurement, the LSF0102DCTR level conversion chip will leak from the high level of the VerfB terminal to the low level of the VerfA terminal. When the VerfB is 3.3V, the EN pin should be connected to 3.3V according to the chip manual. If there is no load, the VerFA terminal should have a voltage of 1.8V, but the measured voltage is around 2.1V. After removing my LDO chip, the voltage is around 2.4V. Is that leakage from VerfB to VerfA? My circuit is like this: