Other Parts Discussed in Thread: CC3301, TXS0206A
Tool/software:
Hi
I'm using TXS0108 for SDIO communication between Microchip DSP 3.3V (ATSAMA5D27C-CNR) and Ti WIFI chip 1.8V (CC3301)
On the 1.8V side I having a 10kohm PU Resistors for all 6 SDIO Signals
When sampling the Signals using Scope I have notice that I the 3.3V Clock that coming from the MPU, and the 1.8V Clock after LS are looking Ok
But when I having a change in one of the DATA or CMD signal, I see a Voltage drop during Clock Rising Up on the 1.8V Clock side
Pic1- Clock looks OK, no change in DATA or CMD:
Pic2- 1.8V Clock voltage drop when CMD signal change
Pic3- 1.8V Clock voltage drop when DATA signal change
Pic4- I also have measured the 1.8V LS Supply during CMD change and it stable
Please advise