Tool/software:
Dear Technical Support Team,
I have a question about SN74LVC1G08.
According to the datasheet , VIL(max) is 0.3 × VCC(=5V)=1.5V, but is TA =25°C or TA=125°C(max),-40℃(min) ?
If it varies with temperature, etc., what is the worst value for VIL when TA = from -40℃(min) to 125°C(max)?
"6.3 Recommended Operating Conditions " doesn't have "over recommended operating free-air temperature range (unless otherwise noted)" such as "6.5 Electrical Characteristics".

Best Regards,
ttd