This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108: TXB0108PWR Is there margin for 1.2V?

Part Number: TXB0108


Tool/software:

Hello Experts,

I am planning to use Vcca = 1.2V, but the power supply may vary due to % error.
Is there any margin for Vcca when using 1.2V?

Thank you.
Filipe

  • According to the datasheet, there is no margin, and 1.199 V would not be guaranteed to work.

    There are typical characteristics for 1.2 V, so I'd guess that 1.2 V ± a little bit would be OK.

    Do you really need an auto-bidirectional translator? What protocol are you using?

  • Hello Clemens,

    The 1.2V is used for FPGA IO pin. Those pin voltage tolerancy is very narrow, also the DCDC may vary +/-% to up or down.
    I am thjinking to chengae the DCDC to ~1.23V or use another level shifter that can handle a wide voltage changes.

    Thank you.
    Filipe