This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G125: Max 5.5V input on /OE pin with VCC 3.3V

Guru 11450 points
Part Number: SN74LVC1G125


Tool/software:

Hello,

My customer asked TI for an answer regarding the maximum input voltage specification for the /OE pin of the SN74LVC1G125.

Is it correct that the /OE pin can be input up to 5.5V when VCC is 3.3V?

Thank you.