Part Number: TPLD801
Tool/software:
Hi Team,
Customer is surveying new deviec to replace AM1U1108 and I found out that TPLD801 migh be a good choice. However, I was wondering if team could kindly help me verify if the function specified below is capable for TPLD801.
Function Requirement:
VDD=5V
IO2: detect if it is being pulled low for more than 3s.
IO3: detect if the status is high
IO6: if both IO3 and IO2 are true, output high after a delay of 2s and keep the status. (default pull down with 10k)
IO7: if both IO3 and IO2 are true, "output low for 100ms and output high" after 3s delay.

Best,
Liang Tsai