Other Parts Discussed in Thread: SN74LVC1G126
Tool/software:
Hello,
I was simulating SN74LVC1G125 in LTspice with output pulled up to 5V through 10kOhm resistor and a toggling input which oscillates at 10kHz.
Since SN74LVC1G125 has tristate behaviour, when the OE is disabled, simulation should show 5V at output pin(owing to pull-up) irrespective of the input. However, the simulation results show logic Low level at output when OE is disabled.
I observed same behavior with SN74LVC1G126 also. Could you please let me know how to correct the model to rectify this error?
Thank you,
Anandhu Raj