Part Number: SN74HC08
Other Parts Discussed in Thread: SN74HCS08
Tool/software:
Hi expert,
My customer is using SN74HC08DR in VFD product and they found three IC broke down when they are under the factory test.

The issue is that pin 2 of SN74HC08 in above schematic is always 0.1V, which will cause the output of pin3 to low voltage level.
They test the impedance between pin1 and pin2 twice, which are 5.23kohm/5.21kohm when IC broke down and the impedance is 6.2Mohm/22.1Mohm when IC is good.


They also did ABA test and new device can fix the issue but issue IC indeed broke down.
Could you please help review the schamtic and find the reason why it broke down.