Part Number: SN74LVC1G175
Other Parts Discussed in Thread: SN74HCS74
Tool/software:
Hi TI,
I have a problem with the 74LVC1G175 which I have being using in a design. After investigating its behavior I have found that it not only changes the output on the rising edge on the clock input, but it also changes the output at the falling edge aswell.The yellow top curve is the clock (pin 1), and the bottom green is the output (pin 4).

Here is a picture of the truth table form the data sheet of SN74LVC1G175DCKR, where it can be seen that only the rising edge should result in changes on the output. 
I am unsure if there are any specific details I should be aware of? It is powered by 3.3V, and coupled as a toggle F-F with a N-channel MOSFET connected between the output and the data input.
Thanks in advance.