Other Parts Discussed in Thread: SN74LVC1G99-Q1, TXU0101-Q1
Tool/software:
Team,
My customer is using the AHCT125 and is concerned about slow inputs (slower than the datasheet max recommended 20ns/V.
Two questions:
1. Can a slow input cause damage to this device or just excessive power consumption?
2. Does the respective "x/OE" pin tied to the "xA" pin remediate this concern. I don't think so since the inputs will still be in the indeterminate state between 0.8 and 2V before /OE puts the output into Hi-Z, but please confirm.
Best regards,
Greg