This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS126: SN74HCS126

Part Number: SN74HCS126
Other Parts Discussed in Thread: SN74AHCT1G125, UCC27517, SN74AHCT125

Tool/software:

Dear TI team,

I am going to use IC- SN74HCS126 to buffer uC 3.3V PWM (Freq- 50 kHz to 500 kHz) to 5V logic level. 

I need to confirm below points;

1. Can this IC work on PWM with mentioned freq? As I am using this between uC and Driver IC of Mosfet, to feed 5V PWM to the Mosfet driver.(3.3v PWM from uC buffered to 5V via this IC- SN74HCS126)

2. What is the minimum Pulse width required in input side to have output ??

Please help with this.