This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G123: SN74LVC1G123DCTR circuit

Part Number: SN74LVC1G123


Tool/software:

Dear TI expert, 

I am working on a project with using SN74LVC1G123DCTR, the target is as following:

1. input control signal(from MCU GPIO or push button), output reset and golden signal, when system power on, reset/golden should be delay to pull high around 10ms, golden should be on first or at same time as reset.

2. when control change from high to low, trigger both reset and golden change from high to low, after sometime, reset change to high first, then golden change to high after a few ms.

I use SN74LV123APWR in the circuit simulation but not use QNOT pin, circuit and simulation result as the picture, VCC2 for inverter has delay, if invertor use VCC directly, reset/ golden will be high immidiately when power on. Could you advice will it work? Thanks in advance!

  • HI AD,

    This looks like it would work. If your delays are a consistent time it might also be worth looking into our new TPLD801 to generate these signals. It would allow you to consolidate a lot of the passives, and discreet inverters into a single 8 pin package.

    Regards,

    Owen