This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] How do I size my external RC components surrounding Auto-Bi Directional Translators to fit my System Requirements?

Part Number: TXB0108TXB0102LSF0102LSF0101TXS0104ELSF0108LSF0002TXB0104TXB0106TXB0101TXS0108ETXS0101TXS0102LSF0204

Tool/software:

Auto Bi-Directional translators demand additional design considerations over other translators, such as external RC loading to ensure compatibility with host/target devices. These level shifters are weak in drive strength due to passFET architectures (LSF, TXS) or weakly dampened outputs (TXB) to be able to support the auto direction capability. With this in mind, system designers need to be mindful of the output loading requirements. The attached excel document can be used to estimate the expected performance/ characteristics.

7536.Auto_Dir_Translators_Calculator_Tool.xlsx

Please note that this tool should not be used as a standalone tool to evaluate performance of the device. Customers should always verify with silicon per their board specifics to ensure SI is appropriate. 

The EVM links below can be used to evaluate the devices:

TXS-EVM

TXB-EVM

LSF-EVM