Tool/software:
I see there are wide ranges for the min and max for the positive going input threshold voltage, and the negative going input threshold voltage. Since this is a dual buffer package, I want to ask if it is possible that one circuit's positive going threshold is on the min side, and the other circuit is on the max side. Or is there consistency between circuits within the same package/IC? Maybe this a general question which can be applied to all multi-circuit IC's.