This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPLD1201: Can the TPLD1201 achieve buffer functionality?

Part Number: TPLD1201


Tool/software:

Hi team, 

Can the TPLD1201 achieve buffer functionality similar to the 74LVC1G07GW?

It seems that the LUT cannot implement this function, so please confirm.

Best regards,

Kyohei

  • Hi Kyohei,

    Yes, it can. You can either connect the input pin directly to an output pin, or make and and gate with both inputs connected to the same signal to make a buffer. To have an open drain output similar to the 74LVC1G07GW, select the output pin, and change the output mode to open drain NMOS.