Part Number: TXB0108
Tool/software:
Dear Voltage-Level Translator Support Team,
Also, among the 8 ports, is there any recommended pin handling for A/B ports in case of unused circuits?
Hiroaki Yuyama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0108
Tool/software:
Dear Voltage-Level Translator Support Team,
Yes, you can add any pull-up/-down resistor to a pin that is always an input.
Unused I/Os can be left open. You can add 100 kΩ pull-downs to ground on both sides if you want to prevent them from having opposite values for a short time during power up; see [FAQ] What should be done with unused I/O pins of the level translator devices?
Hello Jack Guan-san,
Thank you for your reply.
We will respond to customers based on Clemens-san's advice.
Even if the pin is one-way, external pull-up/pull-down should be as recommended in the data sheet and application notes.
Unused I/O pins can be left floating without any problems.