This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC244A: What's the internal pull up and pull down resistor value on output pin?

Part Number: SN74LVC244A


Tool/software:

Hi team,

Customer had a question, during their design, they had 2x SN74LVC244A output pin connect to one bus.

And the input had no pull up or down to control the output logic before the MCU is power up. After the MCU power up, the conflict will be fixed by Software.

The worse case here will be one 244 output 1, and one 244 output 0. Power supply is 3.3V.

Question 1: What's the internal output pull up and pull down resistor value? This is to confirm what's the output voltage level, to check if this will impact the logic.

Question 2: What's the risk if 2x output connect together and one output high and the other one output low?

Thanks.

Regards,

Wesley