This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS72: Holding a Data Bit into Latch

Part Number: SN74HCS72

Tool/software:

Hi E2E Team,

I have below requirement-

1) There is an active low error signal (pulse:  high -> low (100ms) -> high) input to the system

2) There can be a single pulse or multiple pulses based on the pre-defined specification

3) The system requirement is to have an error LED for visual indication and the error LED should be turned on permanently on the 1st falling edge

4) Plan is to drive the error LED enable circuit from a latch because, latch can hold the data at o/p even if the data is changing at the i/p pin

Below are the queries-

1) Please let me know weather SN74HCS72 can be used for the above implementation?

2) Please suggest if there is suitable latch other than SN74HCS72,  which can suffice the above requirement?

3) Is there any other way other to implement the above requirement?

Regards,

Aditya